• What is maximum frequency we can simulate in Sipro?Is there any limitation?

    What is maximum frequency we can simulate in Sipro
    shravan001
    last modified by shravan001
  • Line differential impedance ADS simulation

    Hi everyone!   I'm trying to simulate a pair of microstrip coupled lines, to determine its odd mode impedance and differential impedance, using ADS and, eventually, Momentum. In the end, my point is comparing si...
    emtec001
    last modified by emtec001
  • How to define ground plane in Momentum substrate definition

    Could someone please show me how to properly define the ground plane in the substrate definition of Momentum?  I am trying to do a simple simulation of a 28GHz 50-ohm microstrip/stripline in ADS and compare the S...
    tho
    last modified by tho
  • How much it cost a ADS license

    Hi im interested to adquired a ADS License but i wanna know how much it cost for a studen   somebody can help me?  
    ArathAmavizca
    last modified by ArathAmavizca
  • Change Convergence of Adaptive Freq Sweep

    I'm having a problem using adaptive frequency sweep. The rational fitting model sometimes does not select enough frequencies to accurately model the structure.  The S11 plot below shows where I am getti...
    statusbit
    last modified by statusbit
  • How much it cost a studen license

    Hi i want to know how much it cost a studen license , and the type of support that give a student
    arathamavizcaib
    last modified by arathamavizcaib
  • EMPro, Python, Parameter List

    EMPro Python Scripting: 1. Can EMPro print a report of a design's parameters? If no, is it possible to use Python to print a report of a complex design's parameters? 2. Does EMPro perform design Optimization? If yes...
    Travis
    last modified by Travis
  • EMpro, python, Axial Ratio (dB)

    Want to write python script to get plots of axial ratio in dB, S11, and smith chart of antenna design. Can you help?   Currently takes ~ 8steps to manually drill down to result's AR dB, and that's PER result. W...
    Travis
    created by Travis
  • Importing EMPro circuit component definition from ADS

    Hi,      In EMPro, I usually create a circuit component definition (R,L,C) and assign ports to that definition and select 'not a port' option. However I need to do this every time and fo...
    kroniq
    created by kroniq
  • High Memory Requirement for PCB Simulation

    I'm exporting a PCB design from the Cadence Allegro to ADS 2017.1. The design is a 10 layer board with RF and digital section. I removed the digital fraction so only RF components are remained. Moreover I only export ...
    bijanbina001
    last modified by bijanbina001
  • 2 objects occupying the same space.

    Hi,   New to EPpro. I noticed I never get a warning or error message if I overlapped two pieces of different materials, such as AL and Cu, PVC and FR4, etc. The simulation goes on without a hitch. It'll sta...
    ming.yang
    last modified by ming.yang
  • GCPW model simulation 70GHz in EMPRO

    GCPW simulation @ 70GHz. hello all, I'm currently doing simulation of a GCPW line at 70GHz. But I recently a testboard and the results is far from the simulations.  AFter investigation I suspect some atmospheric...
    OLIVIER_ST38
    last modified by OLIVIER_ST38
  • Where can I find the EMPro's Core Dump file

    Hello, I have been running EMPro 2017 on RedHat 6 for a while. Recently, EMPro starts to crash fairly often. Most of the CAD Tools (such as ADS, Cadence, Matlab) generate a core dump file when they quit. Does EMPro a...
    charlesw
    last modified by charlesw
  • Dissimilarity in FEM Results of Resonant Patch Antenna

    I generally use ADS momentum for circuit design, not used it for Antenna, I usually use HFSS for antenna. I was comparing the results of a microstrip resonant patch antenna designed in HFSS with ADS and EMPro (F...
    Riju
    last modified by Riju
  • emds_mesher.exe CPU usage

      Hi,   Does anyone know why emds_mesher.exe does not use much processing power? I am simulating a fairly big object that has more than 30,000 faces, but it takes forever to finish generating the mesh. Is...
    CChew
    last modified by CChew
  • How to find non-interpolated S-parameters in EMPro?

    Is there a way to view or save the non-interpolated S-parameters of an EMPro simulation?   I've attached example screenshots below where my simulation "converged" from approximately -80 dB isolation to around -2...
    RyanA
    last modified by RyanA
  • EMpro Error Message: attempt to write a readonly database

    Hi,   I keep getting this error message after refining. It says: Attempt to write a read-only database, which doesn't make sense to me. Does anyone know how to fix it?     
    CChew
    last modified by CChew
  • Can radiation pattern of patch antenna integrated with Diode switch and other lumped components be simulated in ADS and EMPro?

    Is it possible to simulate the radiation pattern of the "WHOLE" structure (exactly like the measurement) containing patch antenna and PIN diode switch (using Diode model) and other lumped (R/L/C or .s2p files) element...
    Riju
    last modified by Riju
  • ADS EMPro Connector Example

    I am working through some of the examples to become more familiar w importing EMpro models into ADS and using them for simulation results. Ive started out using the example file ‘EMPro_ADS_handson_wrk’. Fo...
    mberry
    last modified by mberry
  • empro TypeError: PyModule_AddObject() needs non-NULL value

    Any ideas how to resolve this issue? Does EMPro Help tool cover this kind of issue?
    Travis
    last modified by Travis