Skip navigation
All Places > Discussion Forums

EDA Software

Log in to follow, share, and participate in this community.

Recent Activity

Prabhanshu
In the design kit development manual of ADS under the Design Kit Tutorial, there is a item definition code given for a sample_res resistor subcircuit.(Page 234 of 2019 manual or Pg 147 of 2011 manual)(manual is available on website) In that code there are a few AEL functions whose explanation is not given anywhere (either AEL manual or keysight… (Show more)
in EDA Software
AdeK
How can I use PIN diode with patch antenna on ADS for reconfigurable antenna switch?
in EDA Software
fourier54
Click to view contentGenerating Layout with layout->Generate/Update Layout gives the following result  When it should look like this It seems that the layers are "empty". What could be the problem?
in EDA Software
zai_kun_93
Click to view contentHello, I am trying to design a static frequency divider using TAHB analysis. I tried to emulate the design guide example as mentioned in the design guide "DivBy 2 using BJT Sinusoidal Source using TAHB".  This design example is given for a clock frequency of 1GHz. My current requirement is to design for higher frequencies in the D band -mmWave… (Show more)
in EDA Software
RobinC
Click to view contentIt is possible with IBIS AMI models to output internal states as ami parameters. All the SystemVue examples I have seen use parameters as inputs and I haven't been able to work out how to set parameters as outputs. In the AMI Model Specific Parameters tab for the C++ code generator it seems the possibility of parameters as Out might be available… (Show more)
in EDA Software
ZekDe
Click to view contentHi,I am a bit new in ADS and I would like to manage simulate. I added the ODB++ file in ADS and open the SIPro/PIPro and I have 6 mosfet to drive 3 phase BLDC motor. So my question is that 1. I defined High Voltage for supply the motor  VRMs -> HV_LINK is + and GND is - 2.Sink -> Q1( high side Mosfet) -> HV_LINK is + and NetC48_1 is -  now at… (Show more)
in EDA Software
simozz
Click to view contentHi,   I am trying to install ADS on my Linux OS on a /opt/ partition which has enough space to host ADS installation:   Filesystem      Size      Used      Avail      Mounted /dev/sda8       595G      111G      455G       /opt   but ADS does not detect the correct partition available size:       But this is size of the rootfs / partition… (Show more)
in EDA Software
manassé
Click to view content         Hi. I would like to know where to find or install the following transistor in ADS software ?      Thank you in advance for your help!
in EDA Software
PeterRodelco
What is the best way to get a swept frequency response (gain, NF, P1dB, IP3) of a frequency converter using Genesys.
in EDA Software
sc_1234
Hello, I am trying to simulate MIMO_3DChannel model part. I want to get output at its output ports ht and HF. Can anyone please tell me how should I do it? Thanks in advance.
in EDA Software
Load more items