• Reading measurements without interrupting measurement

    Hello, I am attempting to create a program that will setup measurement of the 34465A and continuously send data to PC without interrupting the measurement.   I set up measurement with an infinite trigger, th...
    funkytuqe
    last modified by funkytuqe
  • 34461A DMM data logging with 34980A DAQ

    Hello. I am measuring voltage drop on several DUTs at externally triggered intervals with my Keysight 34980a DAQ and 34922a Multiplexer Module. I want to add operating current measurements, but the Multiplexer Module ...
    Wtec_ZM
    last modified by Wtec_ZM
  • Thermistor for 34420A

    Hello,    I need to measure the ambient temperature with the 34420A and I was planning to use a thermistor,  but I'm not sure what Beta value the thermistor should have.  Please advise.   T...
    GavrilutMircea
    last modified by GavrilutMircea
  • How to activate my 34465A DMM

    Hi  I have purchased a 34465A DMM with the transportable license, Idk how to activate this license on my computer.  Another question is what is the certificated number when I am creating my account? I only...
    sniper_y
    created by sniper_y
  • What are the connectors on the 4339B high resistance meter?

    I've bought a 4339B, which I have not got yet. There are several different connectors on the front, and I could not determine what they are   The interlock connector - perhaps a Lemo of some type ??? The grou...
    drkirkby
    last modified by drkirkby
  • SCPI Error 211 Trigger Ignored

    Hi, I'm trying to take readings quickly via my c# app, but testing out in Command Expert first, my last command causes a SCPI Error "211 Trigger Ignored", I can't find any info about why it was ignored, has anyone res...
    chasher
    last modified by chasher
  • SendSoftwareTrigger 34410

    Hi,   I'm building an app using the IVI-COM drivers using the direct driver instantiation. I am successfully connecting to two DVM's and talking single readings from both, however I now want to trigger with enco...
    chasher
    last modified by chasher
  • configuring 34465A via LAN connection

    Hi all,   I am a Python programmer but I am completely new to this product and to SCPI.   I can successfully connect and read data, change display etc but I am having trouble configuring / seeing my s...
    johnashu
    last modified by johnashu
  • 34461A Simultaneous Measurement?

    Hi,   I have been using the 34461A to measure voltage from an optical power meter. But I now need to measure outputs of two such power meters. Is it possible to use the front and back panel I/Os at the same...
    gsaha10
    last modified by gsaha10
  • 34465A Maximum Sample Rates

    On page 3 of the Digital Multimeters 34460A, 34461A, 34465A (6½ digit), 34470A (7½ digit) Data Sheet it indicates that the maximum reading rate for DC voltage, current and resistance for the 34465A with...
    ealm
    last modified by ealm
  • 34465A with DIG option: strange offset in the sample clock rate

    Hello, I wonder if anybody else has run into this problem, or if an explanation could be found. When using the 34465A for sampling an input signal (using the DIGITIZE and MEM options), the sample rate is consist...
    timop
    last modified by timop
  • U1232A Current Measurement causes voltage drop to device and not work?

    Hi,   I am measuring the current consumption of TI CC2640R2F Launchpad which is powered by 2 AA Batteries. As is it works as expected. However when I connect the Keysight U1232A to measure current, the TI CC2640...
    mtrobregado
    last modified by mtrobregado
  • How to deploy c# project with IVI COM drivers

    So, I've built my app which uses the 34410a dvm drivers, works perfectly from my dev machine, but on another machine, it doesn't run or throw error on event viewer. I guess it's missing something, but the release buil...
    chasher
    last modified by chasher
  • KEYSIGHT 3458A communicaton

    hi i try to communicate with KEYSIGHT 3458A i connected it to my computer with usb to usb A cable and than with prologix adaptor to gpib conect to the ketsight multimeter. i used with teraterm softwear to comunicate a...
    Nir.Zach@solaredge.com
    last modified by Nir.Zach@solaredge.com
  • U1732C SCPI  Commands

    Hello Keysight!   I got a brand new U1732C Handheld LCR Meter. It has a built in IR communication interface, for which I also have the appropriate cable. When setting the cable to 9600 baud, I successfully could...
    Johann Glaser
    last modified by Johann Glaser
  • I have some issues with a 34461A

    I tried to call support but I am in Mexico and the tel. number that used to work and is on your webpage does not work anymore. Is there any voice support directly to Keysight from Mexico?
    theamberco
    last modified by theamberco
  • 34465A Frozen in Error Code

    Hi,   A34465A Error Codes seems to freeze LabVIEW after a few hours of operation.   I never had this before (in the past 3-4 years). We sent out the DMM  for calibration and now it seems to be an issu...
    ForeShadow20
    last modified by ForeShadow20
  • Meterlogger for U1282A

    Hi, I've had a look at this post, (Win10 support for logging s/w ), for additional guidance but still can't get my software to run properly, this is on both an up to date Windows 10 and a Windows 8.1 install. Ba...
    DwightG
    last modified by DwightG
  • U1253B display problem

    Hello and a happy new year,      I have a U1253B multimeter for 5 years now that I love to use because of the oled display. I always had the brightness to the lowest setting. Suddenly the display ...
    saltech
    last modified by saltech
  • Getting a "Trigger Too Fast" error at the end of an AutoCal on a 3458A.

    Nothing is connected to the terminals. I work in a service center and have never seen this error before. Will this need to be sent in to Keysight for repair?
    digitaluser
    created by digitaluser