• What is the confidence level for Keysight DMM specifications?

    For example, the Keysight 3458A 90-day DC Voltage accuracy specification for a 1 V nominal reading in 1 V range would be 4.9 uV. When using this accuracy specification in an uncertainty budget one needs to k...
    JacoEngelbrecht
    last modified by JacoEngelbrecht
  • Is the USB interface of the U2741A modular multimeter optically isolated to prevent ground loops?

    Is the USB interface of the U2741A modular multimeter optically isolated to prevent ground loops?
    e22
    created by e22
  • peak-to-peak is described as cumulative for 34465A but is it really?

    The peak to peak description in the "Compatibility and Differences: 34465A and 34410A..." says it is cumulative in the 34465A model but it does not seem to behave that way. It suggests (and the operating guide uses it...
    cl2
    last modified by cl2
  • 34461A Taking periodic samples

    Hello,   I would like to take periodic measurements spaced 20 ms apart using the 34461A. I am using previous code I wrote for a 34410A but found the 34461A does not have a sampling:source option so you can ...
    JasonAG
    last modified by JasonAG
  • How to use the 2nd display on the 34410A DMM

    This video describes how to setup the 34410A or 34411A Digital Multimeter using the front panel to view the 2nd display. While the main display shows DC Volts, the second display will show you the peak to peak voltage...
    jdwindrvr
    last modified by jdwindrvr
  • Agilent 34401A Digital Multimeter, 6.5 Digit DMM Product Demonstration

    The Agilent 34401A is the industries most popular 6.5 digit digital multimeter. The 34401A is a true multimeter as it offers DCV, ACV, DC and AC current, 2 and 4 wire resistance, frequency, period, diode test and much...
    tomc
    last modified by tomc
  • Problem with switching autorange 34410A

    Hi   I have a multimeter Keysight 34410A. It was used a little.    It have a problem with switching autorange at funcion Resistance. If I switch range mannulaly  2W (ohms) and set autorange It wo...
    OP27
    last modified by OP27
  • PreTrigger count does not seem to work when TrgSrc is Level on 34465A FW A.03.00-02.40-03.00-00.52-02-01

    PreTrigger count does not seem to work when TrgSrc is Level and measuring DCV on 34465A FW A.03.00-02.40-03.00-00.52-02-01 The data acquired starts at the triggering level and not 10000 samples before the triggering ...
    arobgibson
    last modified by arobgibson
  • 34465A Minimum Sample Interval

    This is an observation about the behaviour of the 34465A DMM which is different than the 34411A predecessor. Both DMMs have the DIGITIZING option (standard with the 34411A) and 2M Memory options fitted. When the 344...
    SteveMat
    last modified by SteveMat
  • 34410A - Recording data using VISA, error 410

    Hi,   I am trying to take a large sample of DC current measurements. While the correct readings are displayed on the multimeter itself, the correct data is not being sent to my PC. I only receive the value '16' ...
    mush
    last modified by mush
  • 0V & 0A DC/AC Negative Tolerance (34410A / 34401A)

    What are the negative fluctuations that we expect with preferably the 34410A (or the 34401A) when we are in an open circuit or when a device is turned off for DC&AC Voltage&Current measurements?   I want...
    ForeShadow20
    created by ForeShadow20
  • 3458A memory option -001 ...

    Hello - I have an Agilent 3458A unit (Malaysian built) and want to extend memory with option -001. Normally one needs to replace PAL device U102 with a modified logic content ...   On the Keysight website - the...
    Homer
    last modified by Homer
  • What is Digital Insulation Testers?

    **** Brand digital 31/2 digits Insulation Tester model 954, 5kv multi-range (1kv-2.5kv-5kv) and Insulation up to 200 G???, having a lot of features like Ac Voltage measurement up to 600V, Phase sequence test up to 100...
    mecoinst
    last modified by mecoinst
  • AErr on U1242B

    I recently had a battery leak on my U1242B. I cleaned up the corroded contacts the best I could. I also had one of the contacts on the back of the PCB corrode slightly where the battery cradle contacts touches the mai...
    munkeyjooce
    last modified by munkeyjooce
  • the power adapter specifications of U1252B multimeter

    Could you please tell me the power adapter specifications of U1252B multimeter? Is it just a regular 24 VDC power adapter or is it a special charger?
    dyilmaz
    last modified by dyilmaz
  • 0.0 Ohm measured using 34401A

    Hi, I am using 34401A for 4-wire resistance measurement at the point of contact between gold-plated copper contacts. These contacts are just physically touching under a normal force which varies between 1 to 100...
    LK13
    last modified by LK13
  • U1282A - How to reduce the VSense sensitivity?

    Hello   I had to drill a hole in the wall in potential line of the power line. So I thought of the VSense function of my Keysight - U1282A to check if there are wires hidden in the wall where I want to drill. &#...
    Barny
    last modified by Barny
  • U1272A

    Hello   I have a couple of U1272A devices, that I want to communitcate with using C code. I can see them on my device manager as a com ports.   My question is, where I can find a list of commands to get re...
    ikushnir
    last modified by ikushnir
  • L4534A Selftest - Overvoltage Protection test failed

    Hi at all,     does anyone have detailed information about the Selftest of the L4534A Digitizer? How does the self test works? The overvoltage protection test is sometmes failed, if the unit is in warm con...
    DBD
    last modified by DBD
  • 3458A AC Adjustment with 5700A

    I there. I have a 3458A multimeter that we have repaired, after some errors showing on the display caused by the Dallas NVRAMs and Multislope Rundown and ADC Errors and so on. We switched the 2 dalas NVrams and the on...
    PTCAL
    created by PTCAL