• TestExec SL 7.1.4 - has stopped working

    Hello all....can please somebody help me with one problem : I am using TestExec SL 7.1.4 on a Windows 7, 64 bit and everything is working properly but after when I am closing TxSl Application, almost everytime I am re...
    AlinB001
    last modified by AlinB001
  • how to build a aglient action with Labview?

    hello all, very regret that nobody reply my question. what i want to ask is if i have made a labview style action, must i install labview software so that it can be executed???? thanks!!  
    ccwxh8888
    last modified by ccwxh8888
  • TestExec 7.1.5 External Sequences using MultiUUT

    Hello all. Im working in a MultiUUT testplan that use external sequences, but someone knows how to handle MultiUUT inside the .seqlib file? Its that posible?  
    gerardosanchez
    last modified by gerardosanchez
  • Can the Report be stored automatically?

    I am using this tester in a R&D environment from the testexec develoment environment.  Everyone likes the "report" to store the test results, because it is easily human readable.  Many people have asked ...
    klisjt
    last modified by klisjt
  • Removing Actions with the HP TestExecSL API

    Hello   I have to replace an Action multiple times in several Testplans. So I wont to program a tool with C# and the TestExecSL API in MSVS.   So fare I can add the new Action at the correct position in th...
    pschweiz
    last modified by pschweiz
  • How can i get the form login using the activex in VB.NET ? OPUI

    I write the next function but nothing happens TestExecsl1.security.dologindialog() give me an error Com Exception was unhandled, im trying clicking a button to show the login dialog. I hope you can help me. Thank You...
    pabloint
    last modified by pabloint
  • TxSL Learning Materials

    Hello, I came across TestExec S/W at Agilent website and I am interested to know more. May I know what is the best way to expedite my learning process? Where can I get learning materials? Thanks, Jennifer  
    Jennifer
    last modified by Jennifer
  • error with vee

    error when reinstalling OS windows 7 service pack 1 and reinstalling complete software + vee for hf radio tester. how to rectify this, please help.
    newcomer
    last modified by newcomer
  • Bug or feature: report field <referencing> symbol table

    Hello TestExec Team, I created a report configuration with the "Datalogging Configuration Editor". The report consists of fields which are "referenced to a symbol of this name" in the testplan. If i run a testplan w...
    Juergen
    last modified by Juergen
  • Throughput Multiplier Reporting for cycles > 1

    Hello everybody, I have following Topology: 8 UUTs should be tested with one testplan over many cycles respectively over a loop of time (Menu: Options>Testplan Options>Execution). I enabled the Throughput Mult...
    Juergen
    last modified by Juergen
  • FAQ: TestExec SL Software

    See below the list of FAQ regarding TestExec SL software: 1. The testplan does not run to completion. What is wrong? 2. Can I use NI Labview or LabWindows/CVI with Test Exec SL? 3. What Is the error sequence? When is...
    SweeChye
    last modified by SweeChye
  • How do I optimize a testplan for speed?

    The following techniques can dramatically reduce execution time of a testplan: 1. Use the profiler to determine which actions are taking the most time, either because one action is being called a lot, or because it ...
    SweeChye
    last modified by SweeChye
  • Can TestExec SL support real-time communications?

    I would like to find out about the possibilities of linking TestExec with a real time operation system. Are there any solutions available  for Real Time communication using the TestExec application?  
    SweeChye
    last modified by SweeChye
  • Calling Actions out of Actions

    Hello, considering that I have written a collection of TestExec actions in any programming language e.g. Visual Basic, C or .NET I could come to the idea to reuse code within the action level. So my Idea would be call...
    Hanns
    last modified by Hanns
  • Now Available! Agilent TestExec SL 6.1 Recorded Broadcast

    Missed the live session? :? Not to worry! The WebEx recorded broadcast is now available online. Just log on to www.agilent.com/find/FTevents to explore the new features of the TestExec SL 6.1 - anytime and anyw...
    chinchea
    last modified by chinchea
  • OPUI.NET Example

    Hello, Is there any documentation available about the .Net OPUI example (C:\Program Files\Agilent\TestExec SL 6.1\Examples\OpUI.NET)? I tried to use this example as replacement for the old C++ OPUI, but I get the an...
    SweeChye
    last modified by SweeChye
  • Tracking SCPI (Text Based) Commands used in TestExec Actions

    Hello, for debugging purposes I would like to know if it is possible to track all the SCPI commands issued on a certain instrument by the instrument actions or switching actions (especially operation complete and stat...
    Hanns
    last modified by Hanns
  • Some basic questions

    Hello, i´m using TestExec 6,1 with path 6.1.1. Some parts are currently unclear, maybe someone can help: 1.) How can i use "Run Seleced Steps" when one of the marked part is a "Call"? Currently it seems n...
    OnlyOne
    last modified by OnlyOne
  • Using sub-testgroups

    Hello, this bug will normally never appears... I created a testplan with 90 testgroups where each group is a subgroup of the group before. This works fine up to the group Nr 82 then the text begins to look very stran...
    OnlyOne
    last modified by OnlyOne
  • String-Length off test-names

    Hello, for the next patch you should also limit-check the length of test-names. A name with length >1007 chars shuts down testexec without warning. best regards  
    OnlyOne
    last modified by OnlyOne