• IDC in ADS

    how we can simulate an interdigital capacitor by importing its capacitance equation?
    darya
    last modified by darya
  • 哪里有准确的元件模型呢?

    我们说过模拟要准,必须先要有准确的元件模型。但是哪里有准确的元件模型呢?我们常用的电阻、电容、电感难道有不准的疑虑吗? 是的,的确如此。我们在中学时期学习基础电路用的电阻、电容、电感都是理想值,无论电路的应用频率,元件值都不会改变。但是,射频电路的应用频率到了几百MHz,甚至几个GHz以上,元件会产生寄生效应,不再是单纯的电阻、电容、或电感,而是电阻、电容、或电感的总和,而且元件的特性会随着频率改变。在射频应用领域,通常我们用S参...
    tony_chen@keysight.com
    last modified by tony_chen@keysight.com
  • 仿真准吗?

    我最常被问到的问题就是仿真准吗?大部分的工程师会说,如果没有准确的器件模型,仿真就不会准。 我通常会同意这样的说法。但会加上自己的看法,我的经验里面,仿真是可以是准确的。 电路设计仿真有一个至理名言:垃圾进垃圾出 (Garbage In, Garbage Out)。电路是由许多器件和线路组合而成。的确,如果器件的模型不准确,就别想有一个准确的电路仿真结果。 所以,仿真要准,必须先要有准确的器件模型。
    tony_chen@keysight.com
    last modified by tony_chen@keysight.com
  • 2017Q1_SSO Simulation with Power Aware IBIS Model within ADS

    Labs: IBIS vs. IBIS 5.0 SSO Simulation   Demo:    - EM Modeling of Interconnects and Power    - Distribution Network
    Chih Yuan Tu
    last modified by Chih Yuan Tu
  • 新入职工程师必读课程 - 通信系统 (SystemVue)

    新入职的通信算法工程师、通信系统架构设计工程师以及涉及系统验证的射频工程师,可以使用SystemVue完成通信系统仿真,进行算法开发、架构设计或系统验证,以下为必读的自学材料。   对于算法工程师,建议通过以下课程学习完整通信系统设计流程及更多进阶技巧:   快速入门(基于通信系统): SystemVue 快速入门 - 16QAM 通信系统实现    通信系统设计流程: SystemVue ...
    Jiarui
    last modified by Jiarui
  • 2016Q1_Advanced SI Simulation Skills

    - Lab 1. HSPICE Tx and AMI Rx Co-simulation with ChannelSim - Lab 2. Convert Step Response Waveform to Eye Density with ChannelSim - Lab 3. PCB Transmission Lines EM Modeling with SIPro - ADS2016.01 New Blocks for HSD
    Lin_Ming_Chih
    last modified by Lin_Ming_Chih
  • IC-CAP Python Scripting Series 02: Python API (Dut and Setup)

    This video introduces methods in Dut, Setup, Input, Output and Transform. The example demonstrates how to use get_sweep() method to find sweep order of inputs.
    JasonChen
    last modified by JasonChen
  • OIF GAUI-8 400G PAM4

     Workspace is attached without dataset. Please the design to generate dataset.
    Chih Yuan Tu
    last modified by Chih Yuan Tu
  • Keysight EDA 软件免费学习资源汇总-2019

    本文档提供所有 Keysight EDA 软件(ADS, SystemVue, EMPro, GoldenGate, Genesys, IC-CAP, MBP, MQA, A-LFNA, WaferPro Express, Heatwave)的免费学习资源链接。    内容涉及无线通信(5G/LTE/LTE-A/WLAN...), 射频微波,电磁仿真,天线设计,RFIC, MMIC,...
    Jiarui
    last modified by Jiarui
  • 2019.6.11/13 深圳上海ADS电源完整性仿真与测量训练营资料

    主要内容: PDN设计流程 VRM选择和建模 PDN的测量技术 DC-IR-drop和AC PDN分析 平坦阻抗曲线设计以及DDR电源感知分析 文档资料和设计文件见附件:
    zhangtao
    last modified by zhangtao
  • How to Create an Universal SMD Component Model

    Universal SMD component means this component can be capacitor, inductor, open circuit or short circuit for impedance matching. In this document, the steps to combine multiple s-parameter files into single cell for opt...
    JasonChen
    last modified by JasonChen
  • ICCAP Python Scripting Series 01: Python API (Main and Model)

    This series introduces fundamentals of python scripting in IC-CAP. The video is in Mandarin.
    JasonChen
    last modified by JasonChen
  • Connecting SystemVue to Test Instruments for DPD Measurement

    Product test is one of the most significant step in product development cycle. SystemVue provides connected solution with Instruments to allow product tested with validated source and custom environment. Digital Pre...
    Jiarui
    last modified by Jiarui
  • 新入职工程师必读课程 - IBIS AMI 建模 (SystemVue+ADS)

    IBIS AMI建模对芯片设计人员来说具有一定挑战,既要熟悉电路和信号完整性相关知识,又要具备编程能力;并且随着产品的更新换代,需要不断地重新设计,同时保证每个模型的准确度。   对于新入职或初次接触IBIS AMI建模的工程师,可以使用SystemVue的自动化IBIS AMI建模工具,完成Tx/Rx 均衡算法及Rx 时钟数据恢复等设计及验证,实现自动代码生成,并利用ADS的通道仿真器对生成的IBIS AMI模型进行验...
    Jiarui
    last modified by Jiarui
  • 新入职工程师必读课程 - 半导体器件建模 (Device Modeling)

    新入职的器件建模工程师,对器件建模的概念和流程都缺乏足够了解。通过以下材料可以快速对概念和流程有一个系统的了解,并对工具使用有一定基础。以下为自学材料:   1. 半导体器件建模基础课程--半导体器件建模小课堂 半导体器件建模小课堂1:关于器件建模 Very Basics of Device Modeling 半导体器件建模小课堂2:器件建模的基本流程 半导体器件建模小课堂3:Fitting Flow of MOSFET...
    ShaoliLv
    last modified by ShaoliLv
  • 新入职工程师必读课程 - 信号完整性 (Signal Integrity)

    新入職信號完整性的工程師,可以透過以下的材料自學。 除了粗體字的內容建議先做先看以外,其它都可以依照個人興趣自己安排學習順序。 材料分為workshop和Application Notes: 每個Workshop都有附workspace供操作(約2小時可以完成),請上官網下載最新的ADS,並線上申請試用License。 Application Notes透過影片和文字的方式,帶你快速掌握信號完整性的基本觀念。   W...
    Chih Yuan Tu
    last modified by Chih Yuan Tu
  • ICCAP Python Scripting Series 00: ICCAP Fundamental

    This series introduces fundamentals of python scripting in IC-CAP. The video is in Mandarin.
    JasonChen
    last modified by JasonChen
  • 使用测量波形作为Tx进行channelsim仿真

    参考附件的案例。 注意: 1. 原理图中必须添加变量: “__debug_OutputRedriver=1” 2. 波形文件需要保存成 redriver_wvfm1.txt ,存在data文件夹下。文件格式见附件
    zhangtao
    last modified by zhangtao
  • ADS VTB应用1:5G NR UL包络跟踪仿真分析

    包络跟踪技术是通过跟踪输入信号的幅度,并对功放的偏置进行响应调整,从而提升功率放大器功率附加效率的技术手段。在是德科技EEsof的技术专家Andy Howard的应用笔记中详细介绍了在ADS软件中进行包络跟踪仿真分析的过程,请参考附件中的pdf应用笔记文档和网上研讨会资料。与应用笔记相关的仿真示例请参考EEsof Knowledge Center文档 : http://edadocs.software.keysight....
    xindong
    last modified by xindong
  • 半导体器件建模小课堂5 -- 统计模型(Statistical Model)

    统计模型简介
    ShaoliLv
    last modified by ShaoliLv