• [PDF] Advanced Skill for SI Analysis with ADS in HSD Workshop

    As Title Edited by: Lin_Ming_Chih on Nov 5, 2013 4:54 AM Edited by: Lin_Ming_Chih on Nov 5, 2013 10:48 PM...
    Lin_Ming_Chih
    Bookmarked 7 days ago by Lin_Ming_Chih
  • Python GUI for Data Conversion - Converting ADS Dataset to Touchstone File Format in Batch

    Requirement    The user creates a schematic of SP simulation which has a sweep variable. Thus there're seve...
    Lei_Yue
    Bookmarked 7 days ago by Lei_Yue
  • Oh, the noise! Noise! Noise! Noise*

    Originally posted May 21, 2013   I agree with the Grinch on this one Noise doesn’t undermine everything w...
    benz
    Bookmarked 1 week ago by benz
  • User Defined/Modifying Cal Kit on HP8753ES

    I have a 3.5mm cal kit with different coefficients than the standard kit on the analyzer. I thought It would be a sim...
    sinead9099
    Bookmarked 2 weeks ago by sinead9099
  • Full S-param on high gain device with HP8753ES

    Hi, we would like to read full s-parameters in one time (S11, S22 and S21). The DUT is a 2.2GHz, 50dB of gain (power)...
    demerad
    Bookmarked 2 weeks ago by demerad
  • Custom calibration board on HP8753ES

    Hi, We built a custom calibration kit to calibrate out our RF switch and cable. Below is a picture of it and the VNA...
    wiwyam
    Bookmarked 2 weeks ago by wiwyam
  • HP 8753C Retrofit Option Kits (eg TDR Option 010)

    Dear Colleagues,   I'm trying to understand what is involved in adding Option 010 (TDR) to an HP 8753C network ...
    Apostle
    Bookmarked 2 weeks ago by Apostle
  • Run ADS in Command Line

    Lin_Ming_Chih
    Bookmarked 3 weeks ago by Lin_Ming_Chih
  • Partial Reconfiguration: the backbone of HVI

    Until recent years, synthesis of FPGA images was binary (no pun intended): reconfiguration was an all or nothing sort...
    jakedaly
    Bookmarked 4 weeks ago by jakedaly
  • Keysight EDA 软件免费学习资源汇总

    本文档提供所有 Keysight EDA 软件(ADS, SystemVue, EMPro, GoldenGate, Genesys, IC-CAP, MBP, MQA, A-LFNA, WaferPro Express, ...
    Jiarui
    Bookmarked 4 weeks ago by Jiarui
  • SystemVue 通信实验教程(适用于高校)

    教材作者:中央大学,廖芝青 本教材基于通信原理,通过数字滤波器、BPSK、QPSK、256QAM等实际操作实验,帮助学习者从零开始学习使用SystemVue,适用于高校通信相关实验课,进行辅助教学;也适合需要着手使用SystemVu...
    Jiarui
    Bookmarked 4 weeks ago by Jiarui
  • 2018 Train The Teacher 培训材料(通信/SystemVue部分)

    是德科技大学支持计划   ——2018年度教学培训营 时间:2018年7月30日 - 8月1日      &...
    Jiarui
    Bookmarked 4 weeks ago by Jiarui
  • SystemVue教学材料(通信系统设计)(2017 Train The Teacher培训材料)

    本教学材料包含基于仿真平台的课程指导文件、对应的实验项目文件及参考设计,以及习题示例。   本实验将通过实现基于QPSK 的完整基带/物理层系统设计,帮助设计者快速掌握SystemVue 电子系统级仿真平台的使用,进行通...
    Jiarui
    Bookmarked 4 weeks ago by Jiarui
  • 新入职工程师必读课程 – 三维电磁仿真 (EMPro)

    新入职的射频或是信号完整性工程师,如果需要使用EMPro完成三维电磁仿真,可以通过以下材料自学。 三维电磁场仿真的基础在于建模与仿真器的设定,所以自学材料主要围绕这一部分展开。 如果希望了解更多EMPro应用场景与技巧,可以查看:...
  • 新入职工程师必读课程 - 通信系统(SystemVue)

    新入职的通信算法工程师、通信系统架构设计工程师以及涉及系统验证的射频工程师,可以使用SystemVue完成通信系统仿真,进行算法开发、架构设计或系统验证,以下为必读的自学材料。   对于算法工程师,建议通过以下课程学习完整通...
    Jiarui
    Bookmarked 4 weeks ago by Jiarui
  • Read the current CSA file name from PNA-X using SCPI command

    I am using a PNA-X (5247A), I want to read current CSA file name currently used by PNA-X using SCPI command.  
    waseemahmed
    Bookmarked 1 month ago by waseemahmed
  • Unstable noise display of Agilent 8163B

    The sensor module used with 8163B is 81636B, and the device is driven by a software called IL Engine. After...
    1111112
    Bookmarked 2 months ago by 1111112
  • SIPI Quick Links

    SI/PI Workshops. [SI] FY17Q2 HSD Basic miniWorkshop  Serdes Simulation  Post-layout Simulation: SIPro...
    Chih Yuan Tu
    Bookmarked 3 months ago by Chih Yuan Tu
  • EMPro模擬自動化_用 Python 程式自動運行模擬

    本文作者:中山大学,陈彦伍 EMPro有先进的Python编程环境和丰富的内置函数库。本文通过范例介绍针对已有工程文件如何通过Python程式自动进行电磁仿真或参数扫描。使用该程式可以自动执行任意工程文件的仿真,避免一次又一次在EM...
  • N9912A does not keep the time even reasonably accurately.

    I purchased a used N9912A which had firmware version 5.x and had the wrong date on it - I think it was showing some d...
    drkirkby
    Bookmarked 4 months ago by drkirkby